Quality Control in Electrode Coating
Machine vision detects particles and voids with large amounts of data
![Quality assurance for Electrode coating in Battery cell production](http://images-ctf.baslerweb.com/dg51pdwahxgw/1ZMY84JI6TsSawThQTMk5G/d3e5b8913e499503996359913232b3d5/battery-inspection-coating.webp?fm=webp&f=center&w=800&q=80&fit=pad)
Electrode coating in detail
In electrode coating, the carrier or substrate foil is coated with the previously mixed slurry using an application tool such as a slot die, doctor blade, or anilox roller. The top and bottom sides of the foil can be coated in parallel or sequentially. This is followed by a drying process.
A correctly applied electrode layer has a decisive influence on battery performance
This process step is particularly critical because many parameters must be precisely coordinated: the slurry must have the required stability and be applied at the correct rate. The aim is to achieve perfect coating homogeneity, without cracks or agglomerates, as the electrode layer is particularly important for battery performance.
![Types of defects in electrode production](http://images-ctf.baslerweb.com/dg51pdwahxgw/6hqm4h8zyT379oYmCFNQN5/afe5ef55d8dc77c879e6cd5e31e66b33/batteries-defect-types.webp?fm=webp&f=center&w=800&h=450&q=80&fit=pad)
Possible defects in slurry application
Defects can occur in both intermittent and continuous electrode coating. They depend on the viscosity of the slurry and the accuracy of the dispenser.
Typical defects are:
a. Agglomerate
b. Coating crack
c. Contamination
d. Micro-compression
e. Mud crack
f. Pinhole
g. Slip
h. Stripe
The challenge of large image data
Production speeds of up to 80 m/min and high detail accuracy
Image processing during production presents a dual challenge: very high production speeds, which generate large amounts of image data. At the same time, a high level of detail is required (which is achieved through high image resolution), generating even larger amounts of data. Conventional solutions generally do not have the processing power required to maintain the required production speeds.
Our vision technology ensures reliable quality control in electrode coating
![Quality assurance for Electrode coating in Battery cell production](http://images-ctf.baslerweb.com/dg51pdwahxgw/1ZMY84JI6TsSawThQTMk5G/d3e5b8913e499503996359913232b3d5/battery-inspection-coating.webp?fm=webp&f=center&w=800&h=450&q=80&fit=pad)
![VisualApplets FPGA software for ROI determination](http://images-ctf.baslerweb.com/dg51pdwahxgw/eAD89oW5sqZ7lvF1YZPAs/4b124403411355fd434c196ba68317b2/Screenshot_VA_ROI.webp?fm=webp&f=center&w=800&h=450&q=80&fit=pad)
Only a fraction of the data needs to be analyzed thanks to image pre-processing
The highly-sensitive line scan cameras in our racer and racer 2 series are designed for web material. They deliver the required throughput and image quality for this demanding application. By combining Basler's VisualApplets software and a frame grabber, image data is pre-processed, creating the necessary focus for further image processing. By determining the region of interest (ROI), only the areas with irregularities are localized for inspection—meaning only the image data from the ROI is processed. This allows the CPU of the IPC to continue to be used for the actual system control without any additional load.
![Detection of defect types in electrode coating with the Basler pylon vTool Classification](http://images-ctf.baslerweb.com/dg51pdwahxgw/2NsV95KfWW6Zded2TllcQK/9ec7d8740486037f005cded2091d6e35/Screenshot_defect_classification.webp?fm=webp&f=center&w=800&h=450&q=80&fit=pad)
Classify defects and make qualified decisions with pylon vTools
The next step is to further analyze the irregularities within the ROI. Basler's pylon vTools software can
classify the type of defect or
measure the size of the defect.
Depending on the type and size of the defect, a decision is made as to whether the defect is within tolerance or whether further action is required. Accurate localization and measurement allows for precise removal of defective areas. This improves the quality of the battery cell and minimizes material waste.
Products for this solution
Looking to implement a comparable solution? These products will help you.