Use Case

Cost-Effective Urine Sediment Examination with CNN-Based Vision System

>

What is the CNN-based embedded vision system for urine sediment analysis all about?

In a urine sediment analysis, laboratory employees examine the solid components of a urine sample under microscope to diagnose diseases of the kidney or urinary organs. However, manual examinations under microscope generally carry a risk of errors and take up valuable time. Many laboratories therefore use automated systems. These differ according to the required performance, functionality, and design size, which also means they vary in terms of their integrated vision system. The CNN-based embedded vision system represented below meets the requirements of cost-effectiveness and high-performance.

What are the challenges in urine sediment analysis?

Lab analyses increasingly have to be provided quickly and inexpensively, of course without compromising on reliability. This is possible with a CNN-based analysis algorithm on the right embedded vision system. The decisive factor is the integration of the right hardware and software components—namely those that are coordinated with each other. This is best achieved with an experienced partner.

The solution: a reliable and affordable CNN-based vision system

The demo offers a reliable and inexpensive CNN-based vision system suitable for tasks such as the above-mentioned automated microscopic examination of urine sediment. We carry all required hardware and software components in our extensive portfolio.

The system hardware is composed of a dart color camera module with 5 MP resolution and MIPI CSI2 interface, a suitable data cable, and the Embedded Vision Processing Board developed by Basler. The board provides relevant communication and control interfaces that make it suitable for integration as a central controller unit in small benchtop devices. The core element of our price/performance-optimized board is the i.MX 8M Plus from NXP®. The system software includes the pylon Software Suite, which is used for camera configuration and subsequent image capture and analysis. The dart camera module used has an ISP (Image Signal Processor) that performs all the image pre-processing steps. These include, for example, debayering and denoising as well as setting a ROI (region of interest) and scaling the sensor pixels to the target resolution. Since not all dart camera modules have an integrated ISP, the integrated ISP of the i.MX 8M Plus in the embedded vision processing board can be used as an alternative.

The CNN's subsequent inference is performed on a special processor of the i.MX 8M Plus SoC (System on Chip), known as the NPU (Neural Processing Unit). The computationally intensive tasks typical of CNNs are performed by the NPU with hardware acceleration, which makes execution particularly efficient. The Object Detection pylon AI vTool is optimized for the NPU on the pylon AI platform. After inference by the NPU, further processing steps take place on the CPU (Central Processing Unit) of the i.MX 8M Plus SoC. The pylon Viewer is used to configure the image processing solution: to both configure the output and visualize the bounding boxes using the AI vTool. This allows the urine sediment components to be precisely and efficiently classified and localized in order to generate result statistics. The configuration and the stored recipe can then be transferred to the target application software without any programming effort.

Benefits of a CNN-based embedded vision system in urine sediment analysis:

  • Fully self-sufficient embedded vision processing board—from a single source

  • Board suitable for prototyping as well as series production of your complete system

  • Expertly produced vision technology with long-term availability and price/performance optimization

  • pylon Software Suite offers integrated solutions from image acquisition to image processing and image analysis

  • pylon Object Detection AI vTool for accurately counting and localizing the various urine components

Products for this solution

Looking to implement a comparable solution? These products will help you.

How can we support you?

We will be happy to advise you on product selection and find the right solution for your application.