Technologie capteur

CMOS Sensors: Future-proof Technology

CMOS sensor technology is widely used in industrial image processing. Find out more about the advantages of CMOS sensors, what needs to be considered when integrating CMOS-based cameras and which Basler cameras are equipped with a CMOS sensor.

CMOS cameras dominate industrial image processing
Livre blanc

Quelle est la meilleure façon de comparer les caméras CMOS modernes ?

Dans notre livre blanc, nous comparons les capteurs CMOS modernes. Ce faisant, nous examinons les performances des caméras industrielles avec le même capteur CMOS :

  • Quelles sont les différences pour le fabricant de la caméra lors de l’intégration de nouveaux capteurs CMOS ?

  • Qu’est-ce qui distingue une bonne intégration de capteur CMOS ?

  • Quel rôle jouent les données EMVA dans la qualité de l’image ?

  • Comment vérifier les fonctions du micrologiciel et la stabilité de la transmission des données ?

  • Comment les différences de prix se produisent-elles malgré le même capteur ?

What is a CMOS sensor?

Structure and function of a CMOS sensor

A CMOS sensor (Complementary Metal-Oxide Semiconductor) is used in digital cameras and other devices for image recording. It consists of a matrix of tiny photosensors that convert light into electrical signals. Each light-sensitive cell in a CMOS image sensor has its own charge amplifier. This technology enables – compared to ccd sensors – a significantly higher data transfer rate from the sensor and also leads to an increase in the maximum frame rate of the camera.

Although CMOS sensors used to have a lower sensitivity due to the limitation of the light-sensitive area in favor of the electronics, this is no longer the case today thanks to the implementation of microlens arrays.

CMOS sensors in image processing

CMOS sensors have largely replaced their CCD counterparts in image processing since Sony announced in 2015 that it would cease production of these sensors. Today, CMOS sensors outperform CCD sensors in many areas. With further developments such as Sony's IMX sensor series and Global Shutter and Rolling Shutter sensors, there is the right CMOS camera for almost every application.

Practical examples: Why CMOS sensors are suitable for your application

In our video, our expert Thies Moeller uses practical examples to explain the advantages of this sensor technology for various areas of application, e.g. factory automation, traffic or medicine. Take a look now!

Benefits of cameras with high-performance CMOS sensors

CMOS sensors have improved significantly in recent years, particularly in two important properties of industrial cameras: speed and noise characteristics. In addition, the improvements in CMOS technology and the good price/performance ratio are making CMOS sensors increasingly attractive for applications in industrial image processing. In particular, the very high frame rates with almost constant image quality characterize the current CMOS sensor generation.

What characterizes the latest CMOS sensors

  • High speeds (frame rates)

  • High resolution (number of pixels)

  • Strong dynamic performance

  • Low power consumption

  • Improved noise performance

  • Improved quantum efficiency

  • Improved color concepts

  • Good price/performance ratio

What’s important when integrating the latest CMOS-based cameras?

Integrating a CMOS camera to replace CCD sensors is simpler than expected, especially when you choose standard-compliant hardware and software. Because camera manufacturers take care of the entire sensor integration including image quality optimization, all you need to do when choosing the right CMOS camera is to:

  • Determine the correct resolution of the camera: The required resolution depends on the details you need to make visible in your images.

  • Define the required camera interface: The choice of an interface depends on the required cable length, bandwidth, necessary frame rates and real-time capabilities and PC hardware availability. Our Interface Advisor helps you find the best interface for your application.

  • Choose lens and lighting: Changing the sensor format also involves changing the lens. Our Lens Selector makes finding a new lens easy. Lighting must only be adjusted if the sensitivity of the new sensor is different from the previous one.

  • Integration effort for software and camera control: Cameras complying with common standards such as GenICam, for example, or interface standards like USB3 Vision or GigE Vision, offer uncomplicated integration.

CMOS sensors: Further information on integration

White Paper: Modern CMOS cameras as a replacement for CCD cameras
Livre blanc

Modern CMOS cameras as a replacement for CCD cameras

For more information on switching to CMOS cameras, download our free White Paper "Modern CMOS cameras as a replacement for CCD cameras".

White Paper on the switch to CMOS cameras

Basler cameras with CMOS sensors

The following Basler camera series contain models with CMOS sensors:

Comment pouvons-nous vous aider ?

Nous nous ferons un plaisir de vous conseiller sur le choix des produits et de trouver la bonne solution pour votre application.