New Lighting Control Products
- Date
- 17 Oct 2023
New to our lighting portfolio: multi-channel, cost-effective lighting controllers. Also new: the SLP feature for lighting control is now available for almost all Basler cameras.
Basler's proprietary SLP feature is now available on nearly all Basler camera series, including the ace 2, boost R, ace U, and ace L. Combining a SLP-equipped camera with the Basler SLP Controller enables lighting to be easily integrated into the vision system using pylon software. In particular, the unique automatic flash synchronization can significantly reduce development time on the customer side.
Basler SLP controllers are available in two formats: either already integrated in the lights (the Basler Premium Camera Lights) or used as external controllers (with the Basler Standard Lights). Thanks to the SLP feature, lights can be operated in different modes, including: continuous light, strobing (flash operation), or overdrive (operating with higher light intensity). Soon, the Basler ace 2 X visSWIR cameras will also be equipped with the SLP feature.

Basler is also expanding its vision portfolio with two new cost-effective lighting controllers. The Basler Standard Controllers are available with two (2C) or four (4C) channels to provide lighting control in a vision system. This means a single controller could control up to four lighting systems for one application, saving costs. With the new Basler Lighting Controllers, lighting can be switched to continuous mode or triggered synchronously with the camera (pulsed mode). The lighting control can either be set manually (directly on the hardware) or, in the case of the 4-channel controller, also via a web interface.
The new lighting controllers have already been added to the Basler Illumination Advisor. This is a free online tool designed to be used right at the beginning of the development process to select compatible lighting components matched to the vision system. Users are guided step-by-step to a selection of lighting components tailored to their needs, allowing them to save time.
Download Press Release *.docx (62 kB)
Download Picture (4c, print) *.jpg (1,35 MB)
Download Picture (rgb, online) *.jpg (392 kB)