Frame Rate Calculator - Legacy Version

Frame Rate Calculator legacy

Let the Frame Rate Calculator Do the Math!

The Basler Frame Rate Calculator calculates the frame rate or line scan rate for your Basler area scan camera or line scan camera once a few parameters have been specified. For instance, should you wish to define an area of interest (AOI), the tool determines the maximum frame rate or line scan rate that can be achieved.

We offer the Frame Rate Calculator as an offline version, which you can use on Windows, Linux or macOS. Simply download the tool, unzip it and execute it by a double click.

To use the Frame Rate Calculator please make sure that the Java SE Runtime Environment (JRE) is already installed on your PC: http://java.sun.com/javase/downloads/index.jsp

Download Frame Rate Calculator now

어떻게 도와드릴까요?

제품 선택에 대한 조언을 드리고 고객의 ‍어플리케이션에 적합한 솔루션을 찾아드립니다.