Camera technology

What Is Multispectral Imaging?

Multispectral imaging reveals information that remains hidden to the human eye. But what exactly does multispectral mean? And what impact does this technology have on industrial image processing? We will show you how your vision application can benefit from multispectral cameras.

  • Last updated: 06/01/2023

  • Reading time: approx. 6 Minutes

Webinars

Application examples for multispectral imaging

Multispectral and SWIR technology

In our webinar, we answer the most important questions about multispectral imaging:

  • What is multispectral technology?

  • What can it be used for?

  • Best practice examples

To the multispectral webinar


What are multispectral cameras?

Multispectral cameras are highly specialized industrial imaging devices that see much more than "just" color. They measure image data in specific wavelength ranges of the electromagnetic spectrum, far beyond what the human eye can see (380-780 nanometers). They typically cover 3 to 15 spectral bands, but there are also cameras that can capture hundreds of spectral bands, known as hyperspectral imaging.
These cameras open up new possibilities by visualizing electromagnetic waves with wavelengths outside the visible range, such as infrared. This precise capture of spectral information is helping to improve efficiency and quality assurance in a variety of industries.

These cameras open up completely new possibilities by visualizing electromagnetic waves with wavelengths outside the visible range, such as infrared. This precise capture of spectral information contributes significantly to increased efficiency and quality assurance in various industries.

SWIR and UV in multispectral imaging

Multispectral imaging expands upon traditional image processing by incorporating spectral ranges such as SWIR and UV. SWIR cameras detect radiation in the short-wave infrared range, while UV cameras detect radiation in the ultraviolet spectrum. This makes material properties, surface structures, and details invisible to standard cameras visible.

Some plastics appear transparent in the SWIR spectrum.
Some plastics appear transparent in the SWIR spectrum. By combining multiple spectral bands, even the slightest differences in surface and material properties can be analyzed reliably.

SWIR cameras in multispectral systems

SWIR cameras detect electromagnetic radiation in the short-wave infrared spectrum, typically between approximately 900 and 1,700 nanometers. Using the integrated SWIR sensor, they visualize information that remains hidden to conventional RGB cameras. Materials such as plastics, silicon, water, or organic substances reflect SWIR radiation differently. As a result, these cameras provide precise measurement results for food inspection, moisture analysis, fill level control, material sorting, and the detection of material defects. Key areas of application include industry, agriculture, quality control, and security monitoring.

UV cameras provide significantly more information about the objects being examined than conventional cameras.
UV cameras provide significantly more information about the objects being examined than conventional cameras.

UV cameras in multispectral systems

UV cameras operate in the ultraviolet spectrum and capture information outside the visible light range, typically between about 200 and 400 nanometers. Using a built-in UV sensor, they make surface structures, coatings, or fluorescent materials visible. Even the smallest contaminants, material tensions, or invisible markings can be reliably detected using UV-based multispectral systems. This makes UV cameras particularly well-suited for applications in forensics, the semiconductor industry, medical technology, and scientific analysis.

Options for spectral imaging

There are three ways to obtain spectral image information: a camera with optical elements, a continuous filter such as a filter wheel, or a CMOS sensor with a filter.


Multispectral cameras with optical elements

Multispectral cameras with optical elements

Multispectral cameras with optical elements consist of four main components:

  • Prism:

    Splits the incident light into different wavelengths.

  • Sensor:

    Converts the light into electronic signals.

  • Grating:

    Isolates specific wavebands.

  • Lenses:

    Focus the light for further processing.

Together, these components generate a high-resolution multispectral image. Performance is highly dependent on the precise alignment and calibration of the optical elements, which can be costly.

Filter wheel cameras

Filter wheel cameras


Objects captured with filter wheel cameras are scanned sequentially as the camera captures single wavelengths. For additional wavelengths, the filter wheel must be moved to the desired filter. However, this method has its limitations, especially with moving targets. The slower scanning speed can result in blurred or incomplete images.

CMOS sensor with filter

CMOS sensor with filter


CMOS sensors are now available with bandpass filters integrated into the sensor layout. Unlike other scanning techniques, cameras with spectral filters on CMOS sensors do not require additional optical components to be aligned. They capture objects of different wavelengths in a single image. These sensors are not only less expensive, but also easier to integrate into existing imaging systems.

Overview of multispectral camera applications


Multispectral cameras have evolved in recent years from their original use in aerospace, life sciences and laboratories and are now widely used in other areas, e.g:
Printed circuit boards: Inspection to detect faults and defects
Banking: Counterfeit detection of banknotes
Dermatology: characterization of skin changes and diagnosis of skin diseases.

Focus on multispectral imaging: food industry & agriculture

The main application for multispectral cameras is in the food industry and agriculture.

Multispectral cameras in agriculture

Agriculture

In agriculture, farmers can assess the condition of their crops. Drones equipped with multispectral cameras fly over the field and capture high-resolution images that are transmitted wirelessly to a computer on the ground. By evaluating the data in different colors, such as red and green, farmers can identify diseased plants and treat them with targeted pesticides. This enables the efficient use of resources and protects the environment.

Multispectral cameras in food production

Food production

Multispectral imaging also plays an important role in food production and enables even more precise quality control. Automated processes such as food sorting benefit from the precise detection of foreign objects. While conventional industrial cameras have difficulty distinguishing between debris, stones and dirt, multispectral cameras are able to detect even the smallest deviations.

The future of multispectral imaging

As technology advances and multispectral cameras become more integrated, we can expect even more accurate and reliable analysis in the future, continuously optimizing industrial processes.

Our products with extended spectral range

How can we support you?

We will be happy to advise you on product selection and find the right solution for your application.