analytica 2022: Basler Presents Innovative Computer Vision Solutions for Medical & Life Sciences
- Date
- 5 May 2022
At analytica 2022 from June 21 - 24 in Munich, Basler AG will present the highlights of its product portfolio as well as complete computer vision solutions for medical & life science applications.
Basler AG will present its portfolio for Medical & Life Sciences at analytica 2022 in Munich from June 21 - 24. Under the motto "Let's Realize Your Vision", the company will present its current product lines and comprehensive computer vision solutions for the medical & life sciences market.
As a product highlight, Basler will show the MED ace camera series with its recently optimized MED Feature Set Dust Protection+, which ensures an enhanced level of cleanliness. In applications such as microscopy, dust or other particles can cause interference in the beam path. The Dust Protection+ feature set ensures optimal image quality through improved cleanliness. Basler rounds out its product portfolio with the ace 2, dart, boost, blaze, and 3D stereo camera lines as well as coordinated components such as lenses and processing hardware.
Several practical examples demonstrate the advantage of Basler products in Medical & Life Sciences applications. One demo illustrates an automated microscopic examination of urine sediment using a neural network designed for this purpose and running on an Edge Device. With its computer vision expertise, Basler matches the right hardware and software components with individual customer requirements and offers customized complete solutions from a single source.
In a light microscopy setup, Basler presents how brilliant images can be generated ad hoc with cameras from the MED ace product line using the specially developed MED Feature Sets Brilliant Image and Perfect Color, which are integrated directly into the camera's FPGA.
Marcus Birkenfeld, Global Business Leader Medical & Life Sciences at Basler AG, emphasizes: "For us, communication with our customers is extremely important. After many trade shows were canceled in recent years, we look forward to presenting innovative products and solutions to our customers in personal exchanges."
Basler at analytica 2022: Hall A3, Booth 408
General information on Basler's Medical & Life Sciences portfolio is available at www.baslerweb.com/medical.
Note: Please note that most browsers cannot display 4c pictures. Please right-click picture and select Save Target As... to download and store the picture on your PC. Afterwards, you can view it with an appropriate program.