Dust Protection+: Upgrade of the MED ace Feature Set
- Date
- 8 Feb 2022
The “+” makes all the difference in the new MED Feature Set Dust Protection⁺ for our MED ace camera series: higher cleanliness, better image quality, same price. We accomplish this thanks to such processes as additional and stricter tests of selected components for impurities during assembly.
Available immediately and at no extra charge, you can get eight of the 22 Basler MED ace camera models with the improved MED Feature Set Dust Protection⁺. This feature stands out with its optimized production process, because now we are testing critical components even during the camera assembly. Custom-developed test tools with strict detection limits are used to inspect the sensor and to check the IR cut filter in color cameras and the cover glass in the monochrome cameras. If any impurities are detected, the parts are cleaned before the assembly. During the final review, we once again test the finished camera with the camera test tool. This enables us to reach an even higher degree of cleanliness, which leads to fewer artifacts in the images and thus results in higher image quality and more reliable image analysis. High image quality is particularly crucial for applications such as AI-based classification of objects in an application software, which Basler also offers.
“With Dust Protection⁺, we combine four features that meet the special cleanliness standards often required of cameras by Medical & Life Sciences applications: Sealing of the sensor room, cleanroom production, strictest inspection for dust and other particles as well as high robustness during daily use,” explains Peter Behringer, Head of Medical Business at Basler AG. “This means that Dust Protection+ will particularly benefit customers who use microscopic processes with optical magnifications in their applications.”
Basler MED ace camera designed for medicine, medical technology and life sciences
All models in the Basler MED ace camera series are remarkable for their Basler MED Feature Sets: Easy Compliance, Brilliant Image, Perfect Color, Low Light Imaging, Industrial Excellence, High Speed and Dust Protection⁺. Specifically designed to meet the challenging demands in the Medical & Life Sciences area, the features combine hardware, firmware and software features. They help customers reduce their own development costs by enabling top-quality images in minimal time, while also offering full flexibility for individual requirements.
The color and monochrome cameras in the Basler MED ace series stand out not only with their MED Feature Sets but also with the latest CMOS sensors from the Pregius line by Sony, or the PYTHON line by onsemi. They achieve up to 164 frames per second and have a resolution of up to 20 MP.
Learn more about all the details of the MED Feature Set Dust Protection⁺ and get to know the entire MED ace camera series !