The New VisualApplets 3.3.1 Is Available Now!
- Date
- 12 Apr 2022
Discover the integrated development environment for real-time applications on FPGA processors in image processing. VisualApplets allow FPGAs to be programmed via data flow models on a graphical user interface.
VisualApplets is the integrated development environment for real-time applications on FPGA processors in image processing. This allows FPGAs to be programmed via data flow models on a graphical user interface. The solution is used for industrial and non-industrial applications in a wide range of industries. VisualApplets provides access to the FPGA processors of image processing hardware such as frame grabbers, industrial cameras and image processing devices to enable individual image processing applications.
The new 3.3.1 maintenance release of VisualApplets includes enhancements such as new operators, support for Xilinx UltraScale+ series FPGAs and further improvements.
New operators
A number of new operators for dynamic image shape manipulation have been added. This enables the dynamic cutting or merging of image content at arbitrary positions within the data stream. By that, new classes of image processing algorithms are possible.
Support for Xilinx UltraScale+ series FPGAs
Initial support for devices with Xilinx UltraScale+ series FPGAs has been added, such as the Basler imaWorx CXP-12 Quad frame grabber. This could be especially beneficial for OEM customers looking for customized solutions.
We strongly recommend reading the release notes before updating VisualApplets, to avoid technical complications.
Download VisualApplets 3.3.1Learn more about the features of VisualApplets on our product page