Customer Story

Efficient Warehouse Management with Rapid Pallet Trackers

Artemis Vision relies on the ace camera for barcode capture

Customer
Artemis Vision
Location
Denver, USA
The Basler ace camera in Artemis Vision's Rapid Pallet Tracker vision system uses barcode labels to enable faster and more reliable goods tracking than can be achieved with RFID. For automatic pallet scanning, warehouses benefit from high detection and recognition performance that delivers reproducible results.
Basler ace camera in use in fast pallet trackers
Basler ace camera in use in fast pallet trackers
Robust automated scanning

Robust automated scanning

In warehouse management, high inventory turnover depends on fast and trouble-free goods movements as well as supply chains that can be traced. This is where manual scanning reaches its limits, as it is too time-consuming, slow and prone to errors, which results in too high costs. 

Goods are often moved at high speed both continuously and jerkily, making it difficult to reliably capture the information from a barcode label. This requires fast and robust technology that offers high recognition performance. Scanning barcodes via image processing using the Basler ace camera is a more efficient and much more cost-effective alternative to RFID tracking. 

Basler ace camera for Artemis Vision

Deployed solution 

From each automatic scan in real time with the Basler ace camera acA2440-35um in the Rapid Pallet Tracker, an image with the barcode scan is created. It is time-stamped and stored in a database that can be searched via a web-based dashboard. Such a drive-thru barcode scanning system works without the need for forklift operators to stop or dismount and provides immediate feedback on scanning accuracy. 

We chose this Basler camera model acA2440-35um because of its USB 3.0 interface and IMX264 sensor. Basler cameras stand out because of their competitive price and fast delivery time. Because of their performance, we have had good experience with these cameras in several systems over the years.
Tom Brennan, President Artemis Vision 

Saved loading time and other benefits 

The system saves 25 minutes of loading time per truck, which helps Artemis Vision's customers process more trucks per day. In addition to time, they save money through reduced labor costs and the avoidance of customer penalties and inventory inaccuracies. Compared to the cost of RFID tags, the system can save, at minimum, the cost of one full-time salary per year. Other benefits of RaPTr include: 

  • Requires very little maintenance or space for the equipment 

  • Can be easily integrated into existing ERP systems, but can also be operated independently 

  • Available as a single- or dual-camera model, depending on the size and type of customer barcodes and depending on the warehouse configuration 

Products for this solution

Looking to implement a comparable solution? These products will help you.

Ready to get started together?

Learn more about our products, services, and how we can help you with your next project.